AXIS#.MT.ACC

Description

Specifies motion task acceleration; active in opmode 2 (position) only.

A value of 0 for AXIS#.MT.ACC after a DRV.LOAD command displays an empty (not initialized) motion task.

Examples

Code

Sets the acceleration of motion task 0 to 1000. The first parameter is the motion task number and the second is the acceleration rate.

-->AXIS1.MT.ACC 0 1000

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write Array

Units

Rotary: RPM/s, RPS/s, deg/s2, (custom units)/s2, rad/s2

See Acceleration Units for details.

Range

Depends on units. See Acceleration Units for details.

Default Value

10,000 RPM/s

Depends on units. See Acceleration Units for details.

Data Type

Float

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Commands

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.MT.ACC 0

50d4h

01h

Unsigned32

Acceleration

-

Read/Write

No

AXIS1.MT.ACC 1

50d4h

02h

Unsigned32

Acceleration

-

Read/Write

No

AXIS1.MT.ACC 2

50d4h

03h

Unsigned32

Acceleration

-

Read/Write

No

AXIS1.MT.ACC 3

50d4h

04h

Unsigned32

Acceleration

-

Read/Write

No

AXIS1.MT.ACC 4

50d4h

05h

Unsigned32

Acceleration

-

Read/Write

No

AXIS1.MT.ACC 5

50d4h

06h

Unsigned32

Acceleration

-

Read/Write

No

AXIS1.MT.ACC 6

50d4h

07h

Unsigned32

Acceleration

-

Read/Write

No

AXIS1.MT.ACC 7

50d4h

08h

Unsigned32

Acceleration

-

Read/Write

No

AXIS1.MT.ACC 8

50d4h

09h

Unsigned32

Acceleration

-

Read/Write

No

AXIS1.MT.ACC 9

50d4h

0ah

Unsigned32

Acceleration

-

Read/Write

No

AXIS1.MT.ACC 10

50d4h

0bh

Unsigned32

Acceleration

-

Read/Write

No

AXIS1.MT.ACC 11

50d4h

0ch

Unsigned32

Acceleration

-

Read/Write

No

AXIS1.MT.ACC 12

50d4h

0dh

Unsigned32

Acceleration

-

Read/Write

No

AXIS1.MT.ACC 13

50d4h

0eh

Unsigned32

Acceleration

-

Read/Write

No

AXIS1.MT.ACC 14

50d4h

0fh

Unsigned32

Acceleration

-

Read/Write

No

AXIS1.MT.ACC 15

50d4h

10h

Unsigned32

Acceleration

-

Read/Write

No

AXIS1.MT.ACC 16

50d4h

11h

Unsigned32

Acceleration

-

Read/Write

No

AXIS1.MT.ACC 17

50d4h

12h

Unsigned32

Acceleration

-

Read/Write

No

AXIS1.MT.ACC 18

50d4h

13h

Unsigned32

Acceleration

-

Read/Write

No

AXIS1.MT.ACC 19

50d4h

14h

Unsigned32

Acceleration

-

Read/Write

No

AXIS1.MT.ACC 20

50d4h

15h

Unsigned32

Acceleration

-

Read/Write

No

AXIS1.MT.ACC 21

50d4h

16h

Unsigned32

Acceleration

-

Read/Write

No

AXIS1.MT.ACC 22

50d4h

17h

Unsigned32

Acceleration

-

Read/Write

No

AXIS1.MT.ACC 23

50d4h

18h

Unsigned32

Acceleration

-

Read/Write

No

AXIS1.MT.ACC 24

50d4h

19h

Unsigned32

Acceleration

-

Read/Write

No

AXIS1.MT.ACC 25

50d4h

1ah

Unsigned32

Acceleration

-

Read/Write

No

AXIS1.MT.ACC 26

50d4h

1bh

Unsigned32

Acceleration

-

Read/Write

No

AXIS1.MT.ACC 27

50d4h

1ch

Unsigned32

Acceleration

-

Read/Write

No

AXIS1.MT.ACC 28

50d4h

1dh

Unsigned32

Acceleration

-

Read/Write

No

AXIS1.MT.ACC 29

50d4h

1eh

Unsigned32

Acceleration

-

Read/Write

No

AXIS1.MT.ACC 30

50d4h

1fh

Unsigned32

Acceleration

-

Read/Write

No

AXIS1.MT.ACC 31

50d4h

20h

Unsigned32

Acceleration

-

Read/Write

No

AXIS2.MT.ACC 0

51d4h

01h

Unsigned32

Acceleration

-

Read/Write

No

AXIS2.MT.ACC 1

51d4h

02h

Unsigned32

Acceleration

-

Read/Write

No

AXIS2.MT.ACC 2

51d4h

03h

Unsigned32

Acceleration

-

Read/Write

No

AXIS2.MT.ACC 3

51d4h

04h

Unsigned32

Acceleration

-

Read/Write

No

AXIS2.MT.ACC 4

51d4h

05h

Unsigned32

Acceleration

-

Read/Write

No

AXIS2.MT.ACC 5

51d4h

06h

Unsigned32

Acceleration

-

Read/Write

No

AXIS2.MT.ACC 6

51d4h

07h

Unsigned32

Acceleration

-

Read/Write

No

AXIS2.MT.ACC 7

51d4h

08h

Unsigned32

Acceleration

-

Read/Write

No

AXIS2.MT.ACC 8

51d4h

09h

Unsigned32

Acceleration

-

Read/Write

No

AXIS2.MT.ACC 9

51d4h

0ah

Unsigned32

Acceleration

-

Read/Write

No

AXIS2.MT.ACC 10

51d4h

0bh

Unsigned32

Acceleration

-

Read/Write

No

AXIS2.MT.ACC 11

51d4h

0ch

Unsigned32

Acceleration

-

Read/Write

No

AXIS2.MT.ACC 12

51d4h

0dh

Unsigned32

Acceleration

-

Read/Write

No

AXIS2.MT.ACC 13

51d4h

0eh

Unsigned32

Acceleration

-

Read/Write

No

AXIS2.MT.ACC 14

51d4h

0fh

Unsigned32

Acceleration

-

Read/Write

No

AXIS2.MT.ACC 15

51d4h

10h

Unsigned32

Acceleration

-

Read/Write

No

AXIS2.MT.ACC 16

51d4h

11h

Unsigned32

Acceleration

-

Read/Write

No

AXIS2.MT.ACC 17

51d4h

12h

Unsigned32

Acceleration

-

Read/Write

No

AXIS2.MT.ACC 18

51d4h

13h

Unsigned32

Acceleration

-

Read/Write

No

AXIS2.MT.ACC 19

51d4h

14h

Unsigned32

Acceleration

-

Read/Write

No

AXIS2.MT.ACC 20

51d4h

15h

Unsigned32

Acceleration

-

Read/Write

No

AXIS2.MT.ACC 21

51d4h

16h

Unsigned32

Acceleration

-

Read/Write

No

AXIS2.MT.ACC 22

51d4h

17h

Unsigned32

Acceleration

-

Read/Write

No

AXIS2.MT.ACC 23

51d4h

18h

Unsigned32

Acceleration

-

Read/Write

No

AXIS2.MT.ACC 24

51d4h

19h

Unsigned32

Acceleration

-

Read/Write

No

AXIS2.MT.ACC 25

51d4h

1ah

Unsigned32

Acceleration

-

Read/Write

No

AXIS2.MT.ACC 26

51d4h

1bh

Unsigned32

Acceleration

-

Read/Write

No

AXIS2.MT.ACC 27

51d4h

1ch

Unsigned32

Acceleration

-

Read/Write

No

AXIS2.MT.ACC 28

51d4h

1dh

Unsigned32

Acceleration

-

Read/Write

No

AXIS2.MT.ACC 29

51d4h

1eh

Unsigned32

Acceleration

-

Read/Write

No

AXIS2.MT.ACC 30

51d4h

1fh

Unsigned32

Acceleration

-

Read/Write

No

AXIS2.MT.ACC 31

51d4h

20h

Unsigned32

Acceleration

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.MT.ACC

6300

189C

Unsigned32[32]

Read/Write

Acceleration

AXIS2.MT.ACC

71836

1189

Unsigned32[32]

Read/Write

Acceleration

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.MT.ACC

6300

Float[32]

Read/Write

Acceleration